Hi, I am using 4x ADS805 on a pcb with layout spacing of approximately 21x21mm square. With a ambient temperature of 25 degrees celcius, I measure the temperature on the IC at 50 degrees celcius after a while. The only cooling is a piece of 3mm aluminium glued over the ADS805 with Silicon with normal room air. (For prototypes) Is 50 degrees celcius normal?
The Clk and OE inputs is 5 Volt, with Vdrv at 3V3, and outputs connected to 3V3 FPGA . The Conversion is working fine. Running at 10Mhz constantly. If I switch off the clock, the temperature does not drop. Thanks