Hi,
I have brought TI TSW1266EVM which is connected to an Altera FPGA (Stratix IV)
Can TI provide any initial demo FPGA programming file for using port A of FPGA to receive data from TSW1266 EVM?
Thanks,
Anthony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have brought TI TSW1266EVM which is connected to an Altera FPGA (Stratix IV)
Can TI provide any initial demo FPGA programming file for using port A of FPGA to receive data from TSW1266 EVM?
Thanks,
Anthony
Hi Jim
The HSMC-ADC-BRIDGE, which I brought from TI, have some difference to one ARRIA-TI-ADAPTER.
Odd number of the pins is directly short to ground, Thus, I can't receive both signals from dual channels of TSW1266.
Also, The ARRIA-TI-ADAPTER is unavailable now.
SO, How can i get a correct bridge to connect the TSW1266 and FPGA's HSMC?
Best,
Anthony
Anthony,
This project was taken over by Arrow. You may want to contact them about getting this board. On the latest version, the ASP part number you mentioned was changed to QTH-090-02-F-D. The board database can be downloaded from the link below.
Regards,
Jim
Anthony,
The ADS5402EVM is designed to plug directly into the TSW1400EVM. At one time, new connectors were used which added mounting posts. Once in a while, we get customers who received one board with these post and one without which prevented them from mating. In this case, we instructed them to cut off the posts, or send us the board and we would do this for them or we would swap out the connector. Is this your situation?
Regards,
Jim
FAB_DATA_HSMC_ADC_BRIDGE_REV_C.zipASSY_DATA_HSMC_ADC_BRIDGE_REV_C.zipAnthony,
May I ask what project or development this is for? The files are attached.
Regards,
Jim
Jim,
Thank you so much and sorry for the late reply.
I am doing the research on digital predistortion such that I need to receive a 12-bit resolution ADC data from receiver. then processing inside the Stratix IV FPGA
Actually, the setup is just like the receive part of TSW1400EVM, If you have this part of code, can you also send it to me to simplify my job?
Best,
Anthony