Hi ,
I am trying to load customized firmware to MSP430 on the AFE4490 EVM for testing purpose. Also I am desiging a GUI to receive and visualize the data.
But there are two emergent questions, can you please take a look at them? Thanks.
1) Can I use the ' MSP430 USB Debugging Interface: MSP-FET430UIF' to download the firmware to the board?
But MSP-FET430UIF has 14-bit interface, and the debug interface on the AFE4490 EVM is 10-bit. Not sure why it is like this?
2) For PC side, should I use 'Code Composer Studio (CCS) ' or 'IAR' to perform simulation and project building?
3) Is there material showing how to get data from EVM to PC vis USB?
Much appreciated !!
Best,
Qi