hi,
i am connecting the ADC12J4000 to virtex 7 and are currently facing some problems receiving correct data at the receiver.
when i set the adc to short transport test mode, i will receive correct data in Lane 01,2,4,5 and 6. however lane3 and lane 7's data is always not correct. when is switch to ramp test mode, error also occur in lane3 and lane7.
Below is the configuration of the ADC and receiver core:
ADC
Fs = 4GHz
K=4
F=8
L=8
D = 1 (DDC bypassed)
DDR : 1 (DDR Rate)
P54 : 0 (5/4 PLL Disabled)
Sysref = 25MHz
receiver
Xilinx JESD204 v6.1 (virtex 7)
GT Ref clock = 200MHz
Sysref = 25MHz
Any idea what is wrong?