Other Parts Discussed in Thread: DAC1220
Im using DAC1220 for my project. I have generated the DAC_CLK and DAC_SCLK from the FPGA clock which is 10MHZ.
After this a delay of 100us is generated, in this Delay the DAC_SLCK and DAC_CLK is set to '0'.
After the delay is completed i have made a signal pin that is set to '1'. This pin I am using for starting the process of sending the data to SDIO after the delay.
Falling edge of the SDIO a count is started so that at each count the bits of INSR1(for CMR),CMR1,CMR2,INSR2(for DIR),DIR is send.
1. I am sending the INSR1 for the CMR (MB = 01(2 bytes) and A3 A2 A1 A0(0101)), thus DAC will interpret that CMR is selected the the next 8 bits will the instruction for CMR1,then i am sending the CMR1(10111100) which has BD is '1' which means that the address will be decremented.
2. Then DAC will decrement the address and the wait for instruction for the CMR2 thus i send the CMR2(11100000) . after this I am sending the instruction to jump in the DIR address through INSR2(01000010) which has MB= 10(3 bytes) and A3 A2 A1 A0 = 0010 and then i send the data for conversion to the DIR of 24 bits through the SDIO. after this i am ending the the process and if statement which i was using to check the each count value and on that count i was sending bits to SDIO i.e. I am running this only one time not repeatdly
I am sending the INSR1,CMR1,CMR2,INSR2,DIR of 24 bits to the sdio at each count (the count which is incremented at falling edge of DAC_SCLK).
Now my doubts are whether the A3 A2 A1 A0 is to be set in the INSR1,INSR2 as it is not mentioned anywhere? If i am stopping the process after one conversion i am still getting the repeated pattern on the SDIO pin.
And if i changed the DATA of DIR(24 bits for conversion) i am still getting the same voltage at VOUT = vref, showing no change if the digital bits of DIR are changed.
For repeated proecess whether i have to send the INSR1,CMR1,CMR2,INSR2 repeatedly and only once?
The main problem is in simulation i am obtaining the results on SDIO one time means only for one conversion bits are shown but in real approach i am getting the repeated patterns which it was supposed to be send only one time. I tried it to send on some random pin of FPGA in that also repeated pattern is generated.
Can you go through my program and help me in this. If my interpretations are wrong somewhere please guide me in that.
i am attaching the vhdl code for it and the schematic of device.
THANK YOU.
----------------------------------------------------------------------------------
-- Company:
-- Engineer:
--
-- Create Date: 16:44:27 05/10/2016
-- Design Name:
-- Module Name: dac_sts - Behavioral
-- Project Name:
-- Target Devices:
-- Tool versions:
-- Description:
--
-- Dependencies:
--
-- Revision:
-- Revision 0.01 - File Created
-- Additional Comments:
--
----------------------------------------------------------------------------------
library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.STD_LOGIC_ARITH.ALL;
use IEEE.STD_LOGIC_UNSIGNED.ALL;
use IEEE.numeric_std.ALL;
-- Uncomment the following library declaration if using
-- arithmetic functions with Signed or Unsigned values
--use IEEE.NUMERIC_STD.ALL;
-- Uncomment the following library declaration if instantiating
-- any Xilinx primitives in this code.
--library UNISIM;
--use UNISIM.VComponents.all;
entity dac_sts is
Port ( CLK_CRY : in STD_LOGIC;
DAC_SCLK,DAC_CLK : out STD_LOGIC;
DAC_CS : OUT STD_LOGIC := '0';
GPIO_OUT : OUT STD_LOGIC_VECTOR(23 DOWNTO 0) ;
DAC_SDIO : inout std_logic
);
end dac_sts;
architecture Behavioral of dac_sts is
signal dac_count: std_logic_vector(24 downto 0) := "0000000000000000000000000";
signal dac_cnt,dac_cot : integer range 0 to 95 := 0;
signal dac_delay : integer range 0 to 10000 := 0;
signal pn,pn1,pin : std_logic := '0';
signal dac_sclk_cntr : std_logic := '0';
SIGNAL adc_reg : STD_LOGIC_VECTOR(23 DOWNTO 0) := "000000000000000000000000";
begin
process(CLK_CRY)
begin
if rising_edge(CLK_CRY) then
dac_count<= dac_count+ 1;
dac_delay <= dac_delay + 1;
end if;
DAC_CLK <= dac_count(1);
DAC_SCLK <= dac_count(4);
dac_sclk_cntr <= dac_count(4);
if dac_delay <= 1000 then
DAC_SCLK <= '0';
DAC_CLK <= '0';
elsif dac_delay > 1000 then
pn <= '1';
end if;
end process;
process(CLK_CRY,dac_sclk_cntr)
begin
if pn = '1' then
if falling_edge(dac_sclk_cntr) then
dac_cnt <= dac_cnt + 1;
end if;
end if;
if dac_cnt = 1 then
DAC_SDIO <= '0';
elsif dac_cnt = 2 then
DAC_SDIO <= '0';
elsif dac_cnt = 3 then
DAC_SDIO <= '1';
elsif dac_cnt = 4 then
DAC_SDIO <= '0';
elsif dac_cnt = 5 then
DAC_SDIO <= '0';
elsif dac_cnt = 6 then
DAC_SDIO <= '1';
elsif dac_cnt = 7 then
DAC_SDIO <= '0';
elsif dac_cnt = 8 then
DAC_SDIO <= '1';
-----------------------------------------------------------
elsif dac_cnt = 9 then
DAC_SDIO <= '1';
elsif dac_cnt = 10 then
DAC_SDIO <= '0';
elsif dac_cnt = 11 then
DAC_SDIO <= '1';
elsif dac_cnt = 12 then
DAC_SDIO <= '1';
elsif dac_cnt = 13 then
DAC_SDIO <= '1';
elsif dac_cnt = 14 then
DAC_SDIO <= '1';
elsif dac_cnt = 15 then
DAC_SDIO <= '0';
elsif dac_cnt = 16 then
DAC_SDIO <= '0';
------------------------------------
elsif dac_cnt = 17 then
DAC_SDIO <= '1';
elsif dac_cnt = 18 then
DAC_SDIO <= '1';
elsif dac_cnt = 19 then
DAC_SDIO <= '1';
elsif dac_cnt = 20 then
DAC_SDIO <= '0';
elsif dac_cnt = 21 then
DAC_SDIO <= '0';
elsif dac_cnt = 22 then
DAC_SDIO <= '0';
elsif dac_cnt = 23 then
DAC_SDIO <= '0';
elsif dac_cnt = 24 then
DAC_SDIO <= '0';
----------************insr for dir************---------------
elsif dac_cnt = 25 then
DAC_SDIO <= '0';
elsif dac_cnt = 26 then
DAC_SDIO <= '1';
elsif dac_cnt = 27 then
DAC_SDIO <= '0';
elsif dac_cnt = 28 then
DAC_SDIO <= '0';
elsif dac_cnt = 29 then
DAC_SDIO <= '0';
elsif dac_cnt = 30 then
DAC_SDIO <= '0';
elsif dac_cnt = 31 then
DAC_SDIO <= '1';
elsif dac_cnt = 32 then
DAC_SDIO <= '0';
----------------------------------------------
elsif dac_cnt = 33 then
DAC_SDIO <= '1';
elsif dac_cnt = 34 then
DAC_SDIO <= '1';
elsif dac_cnt = 35 then
DAC_SDIO <= '1';
elsif dac_cnt = 36 then
DAC_SDIO <= '1';
elsif dac_cnt = 37 then
DAC_SDIO <= '1';
elsif dac_cnt = 38 then
DAC_SDIO <= '1';
elsif dac_cnt = 39 then
DAC_SDIO <= '1';
elsif dac_cnt = 40 then
DAC_SDIO <= '1';
elsif dac_cnt = 41 then
DAC_SDIO <= '1';
elsif dac_cnt = 42 then
DAC_SDIO <= '0';
elsif dac_cnt = 43 then
DAC_SDIO <= '0';
elsif dac_cnt = 44 then
DAC_SDIO <= '0';
elsif dac_cnt = 45 then
DAC_SDIO <= '0';
elsif dac_cnt = 46 then
DAC_SDIO <= '0';
elsif dac_cnt = 47 then
DAC_SDIO <= '0';
elsif dac_cnt = 48 then
DAC_SDIO <= '0';
elsif dac_cnt = 49 then
DAC_SDIO <= '0';
elsif dac_cnt = 50 then
DAC_SDIO <= '1';
elsif dac_cnt = 51 then
DAC_SDIO <= '1';
elsif dac_cnt = 52 then
DAC_SDIO <= '1';
elsif dac_cnt = 53 then
DAC_SDIO <= '1';
elsif dac_cnt = 54 then
DAC_SDIO <= '1';
elsif dac_cnt = 55 then
DAC_SDIO <= '1';
elsif dac_cnt = 56 then
DAC_SDIO <= '1';
else
DAC_SDIO <= '0';
-- pn <= '0';
end if;
end process;
end Behavioral;