Other Parts Discussed in Thread: ADS8320, OPA320, MUX36S08, OPA365
Hi,
I am using ADS8320 in an application to monitor temperature and voltage. An 8 channel analog multiplexer is used to switch 6 temperature sensor voltage and 2 channels to measure 3.3V (V1 and V2). The sequence of reading is, firstly read channel 0 to channel 5 of thermistor which is of 360mV and then V1 and V2. This cycle repeats. So every time after reading the V2 and then reading the Channel 0, there is around 35 adc count difference. All other reading values are proper.
After enable the multiplexer there is enough delay (200 uS) provided before enabling the chip select of ADC.ADC is working at the full speed.Looks like after reading the high voltage (3.3V) and then read the other signal the issue is occurring.Please provide some insight on this.
ADC read value: 48570, 48550, 5324, 5288, 5289, 5288,5288, 5288, 48561, 48537, 5325, 5288, 5289, 5288, 5288, 5288.....
Thanks,
Akhil