Part Number: ADS7828
Hi, everyone.
I am using the IC ADS7828EB for ADC. It in the single mode with the external reference voltage of 3.3V, and COM connected to GND. My problem is when I set command byte for ch0 or ch1 with internal reference voltage OFF of and ADC conversion ON, the input does not sense correctly. An always get the value between 3200 and 3400 bits on I2C bus. It doesn't matter if the input voltage is 0 or 3.3V on the channel.
Please advice.