Part Number: ADS7828
I am using ADS7828EB/2K5 in my design to measure external voltages but my readings fluctuate because the IC's Vdd (+5V) changes +- 0.1V. Is there a way I can measure Vdd or measure the chips internal voltage reference (2.5V) to then calculate what my true Vdd is and then use a more accurate Vdd in my software? In summary, I would like to gather a more accurate Vdd to use in my software instead of a fixed 5.00 V.
sheet, how are we able to address pin 10's voltage? I only see how you can ask for Ch0-Ch7 voltages.