Hello ,
I use Xilinx FPGA and the DAC39J84 to establish the JESD204B developing environment.The basic configuration are as follows:
10Gbps, L=8, M=4, S=1, HD=1, K=32. I choose to use both the DAC PLL and Serdes PLL ,and I'm sure The two PLL are locked by reading the register config108(0x6C) . And when I read the state registers (config100——config107) , all of them gave me the same feedback——“”“read request with empty FIFO”. And I can't get any data from the IOUT pins.
Can you help me about this question?
Thanks!
Yours,
Christine