Part Number: ADS4122
Other Parts Discussed in Thread: THS4541, TIDA-00942, OPA656
Hi all,
I am working on a project in which I need to sample and convert a 1.5MHz signal. I was hoping to find a microcontroller with a built-in fast enough ADC for this task but it is very hard to find uC with ADCs capable of more than 5 msps, which is definitely not enough for my application.
I decided then to explore the option of using an external high speed ADC, and based on speed, resolution and cost I found the ADS1422 a reasonable option.
The question I have is whether it is possible to interface a converter like this directly to a microcontroller? I can see that FPGAs are usually employed for this task. I reckon this has to do with the fact that most high speed ADCs provide differential LVDS outputs that microcontrollers cannot interface directly with, but the ADS1422 also provides de option of single-ended LVCMOS output. Is there also a timing issue, e.g., the data valid time at the ADC output? Would a buffer/data latch be needed?
Any help on this would be welcome!
Thanks!
Pablo