This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are trying to measure ECG and Respiratory rate at the same time with ADS1292R but only using the two arm leads(ELA and ERA). We've looked at the suggested application schematics provided in the Evaluation Kit datasheet (attached below), but that design uses all four leads, so how to configure and connect the RLDIN, RLDOUT, and RLDREF pins is one of the problems we have at this stage.
The other problem we are facing is how to detect lead-off with noise as low as possible. In one of our previous designs, we only used the two arm leads for measuring ECG signals, but the noise for lead-off detection part was so large that we had to make an external lead-off detector through software methods. The configuration is attached here. So is there any ways to configure the lead-off detection automatically using merely the ADS1292R chip under the circumstance that we want to measure ECG and Respiratory rate at the same time using the two arm leads?
Thanks a lot!
Hi Jingyi,
If you are AC coupling your inputs, you can just leave RLD_OUT floating.