Team,
My customer is asking:
We are looking into RFDACS. I’m aware of built in interpolation, and new mix modes to get signals in higher nyquist modes.
Is there a design or planning document to work out the process?
E.G. we have a 45 and 75MHz bandwidth signals. We want to use a single RFDAC to output in 700-900, 1700-1900, 2100, and 2600MHz bands.
This would dramatically simplify the up-conversion and with the exception of post filters, we might be able to use the same hardware.
Any reference, or guidance would be greatly appreciated.
Thanks
Viktorija