This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I would like to test ADS1293 functionality by connecting ADS1293 EVM SPI pins to SMARTRF06 board.
I removed JP2 and JP3 jumbpers on ADS1293_EVM and applying external power source on VDD_INP jumper. I am using J2 connector to interface SPI and IOs from CC2650 SMARTRF06 board.
But ADS1293 is not working properly, sometimes it sends data and sometimes it stops working suddenly.
Can ADS1293 EVM really be used with external processors?
Is there any care to be taken when we do this?
Any help will be highly appreciated.
Regards
Lakshmikanth