I am using ADS1232 for weigh scale application. Output of loadcell is 2mV/V.
Excitation voltage -- 5V, Samples per second -- 10nos.
Gain = 64
Above parameters are set for ADC. At present I am masking 4 LSB and the result of conversion has fluctuations of @ 200 in raw counts.
I tried moving average algo but still results are not satisfactory.
When I use 5 kg weight which is displayed as 5000; the last digit fluctuates by 2.
Is FIR filter required for additional stability. If yes can you suggest me the parameters for filter.
I am trying for 6 readings(order).
Thanks
S Agashe