Part Number: DAC8563
Other Parts Discussed in Thread: ADS8568
Hello,
I am interested in using DAC8563 for my project. I want to be able to get +-2.5 V bipolar output for both of the output channels of DAC5863 with +2.5V external reference voltage. Although ithe bipolar output configuration is stated in the datasheet, the explanation is still unclear for me. As far as what I understand from the datasheet the following configuration should be implemented:
However I am not entirely sure if this is the correct one (or I would come up with an easier one).
Also if there is any C/C++ code for DAC8563, could you please help me to obtain that?
Thanks in advance,
Handenur Caliskan