Part Number: ADS54J60EVM
Other Parts Discussed in Thread: ADS54J60, LMK04828
Symptom
I am noticing something strange in sampled data - least significant byte of the 16-bit ADC samples seems to the same as sign bit! This happens regardless of the amplitude of the signal sent to the ADC, or even when no signal is connected to the ADS54J60EVM input ports.
I wanted to run this by you all in case someone has seen this during their bring up of the ADS54J60. Any ideas why bits [7:0] as highlighted in figure [1] below seem to be exactly the same as bit [15]?
This behavior seems to reduce the resolution, but I am still able to observe a sine wave [3].
Configuration
My configuration settings are as follows. I have also attached the two config files that I am using to program the ADS54J60 EVM (LMK04828 and ADS54J60 parts).
Fs = 819.2 MHz
LMFS = 8224
K = 16
Subclass = 1
SYSREF = 3.2 MHz (Enabled)
Figures
[1]
[2]
256-bit output from Xilinx JESD204 core at 102.4 MHz. 8 lanes x 32 bit datapath = 256 bits
[3]