Part Number: ADS1248
Other Parts Discussed in Thread: ADS1218, SN74LVC2G157, PCA9535
Hi,
I configured the ADS1248 to power down mode by taking the START pin to low.
VDD is connected to 3.0V and AVD is floating (The analog power was shut down).
According to the datasheet I should expect a current les then 1uA over the VDD however the current is 200uA. (When I disconnect the 3.0V from VDD the current drop by 200uA)
Any idea why the current is that high?
Attached is the ADS1248 schematic.
Thanks
Noam