Hi, I'm EMC testing a product which uses the TVP5154 ( not the TVP5154A ) to decode PAL video and it seems particularly susceptible to conducted interference on the video input/output and mains cables at multiples of 15.625kHz ( most notably 156.25kHz )
The test uses a current injection probe clamped around the video input coax cable to induce a sinewave interfering signal into it: At low amplitudes of interfering signal the video image becomes heavily patterned and then the TVP5154 loses the line sync well within the amplitude limits of the test signal.
It seems pretty clear that the interfering signal is messing up the line sync detection in the TVP5154 when it is a multiple of the line sync rate.
The video input connector and and the mains earth are both well bonded to the product chassis - this normally helps protect the video signal from interference applied in this way but does not help in this case.
Are there any particular factors I could look at which could help increase the immunity of the sync detection in the TVP5154?