Part Number: ADS8317
Hi,
I have a customer using ADS8317 in their products.
Waveform jumps when output code is near zero.
ADS8317 Data Sheet P.16 THEORY OF OPERATION
I found the following description.
Differential linearity for the ADS8317 is factory-adjusted via a package-level trim procedure.
The state of the trim elements is stored in non-volatile memory and is continuously updated
after each acquisition cycle, just prior to the start of the successive approximation operation.
■Question
Is there a possibility that the adjustment value of the internal non-volatile memory is erased
or changed?
For example, is it caused by the following?
・Logical sequence
・Logical interface
・Power sequence
・Signal level
Best regards,
Seishin