Hi all,
I'm using the ADC32RF45EVM eval board with the TSW14J10EVM interposer and the Xilinx ZC706 board. Having a problem seeing data in the HSDC GUI, getting a ADC to DDR timeout, implying data wasn't collected or stored.
I've programmed the ZC706 Zynq device with the supplied bitfile successfully. There isn't a single reference document showing ADC32RF45EVM configuration for the ZC706 using the 14J10 interposer, so I used TI's KCU105 guide for setting up the ADC32RF45EVM's configuration. I've got external clocking going to J5 and J7, 2GHz 12dBm. After making the appropriate settings in the ADC32RF45EVM software, I get all three LCR blinking LEDs on the ZC706, indicating that the clocks are working. A test signal taht's 600MHz 6dBm is going into Channel A input.
Is there anything else I should be doing in order to see spectrum? Is there a specific guide that targets this particular combination of ZC706 and ADC32RF45EVM?
Thanks!