Other Parts Discussed in Thread: DAC9881
I would like to construct very clean microcontroller progrogrammable supply with output current max. 50mA and voltage range up to 32V. Main source is battery, which is boosted to 36V with DC/DC (LM7233), which is followed by linear post-reg to filter out ripple and stabilize output voltage at desired level.Output voltage range should be from 20V (0V not required, it is handled by enable of the DC/DC). Step size/resolution should be as small as possible.
I was thinking to place MDAC in feedback of a low noise/high PSRR linear regulator, something like this:
Is this idea OK ?
Thanks for any suggestions,
Marko