Part Number: ADS7961
Other Parts Discussed in Thread: TLC2543, , , ADCPRO
Reissuing a percussion sound module and updating the trigger inputs. Was using a TLC2543 but need a DAC with all the same specs but min 14 channels.
Looking for the following:
- SAR Analog to Digital converter
- multi-channel muxed input
- 13+ channels
- single-ended conversion
- up to 5V operation
- 8-bit resolution
- SPI interface
- must be able to read in 8 SPI/serial clock cycles
Is there a work around for either the ADS 7961SRHBT or ADS 7961QDBTRQ1, that will allow us to reduce the SCC to 8?