This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using ADS4249 EVM. The board has CDCE72010 as clock jitter cleaner.
However, on this movie:
I see that they use TSW4806 EVM which includes LMK04806B clock jitter cleaner.
The LMK04806B chip is cheaper than the CDCE72010 chip. I wonder if CDCE72010 has any better features over the other one?
Which one of them will perform better if a use a FPGA generated clock of 840 MHz. in order to create ADC clock of 210 MHz?