This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I have read the user guide of this evm board and also the datasheet of ADS5263.
I found the evm board provide two ac-coupled drivers for ADC.
One is transformer based and another one is an amplifier with a bandpass filter. Can I bypass the bandpass filter of the driver to get an input band start from DC?
And the datasheet of ADS5263 said it has a Low-Frequency Noise Suppression Mode, can I disable the mode to ensure my low-frequency input signal to be sampled by the ADC?
Thanks!
Zhuang
Hi Praveen
Thanks for your reply. For my application, it requires sampling a signal which has a low-frequency component around 60Hz and also high-frequency components from 200KHz to 1MHz. I want to choose a fast ADC to sample this signal as accurate as possible and also can be connected to FPGA by HSMC or GPIO connector.
Thanks
Zhuang