Part Number: ADS1298ECGFE-PDK
Hi,
This is probably linked to the same thread title.
I am also using the ADS1298ECG-PDK evaluation board with software "ads129xecg-fe-setup-1.1.1.exe" from the ftp site (ftp.ti.com/.../ADS1298/ads129xecg-fe-setup-1.1.1.exe/).
As part of our evaluation tests we would like some additional options. The primary one is to change the notch filter at the ECG post analysis section. The notch filter has only two options. 50HZ and 60Hz and we would like to set another value , like 2,5,10,15,20 Hz to test them out. Is it possible and how ?
I thought that maybe having the source code for ADS1298ECG-PDK would help.
In other posts i have seen that they mention the file Source_ads129x_v1p1p1A.zip. However, the source code cannot be found in the FTP.
I would appreciate having the instructions / config file and/or the source code for ADS1298ECG-PDK with instructions how to change the notch filter settings, specifically the center frequency in the ECG analysis window section.
Thanks for your help.
JD