This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8698EVM-PDK: Issues to communicate withe the ADS8698EVM-PDK

Part Number: ADS8698EVM-PDK
Other Parts Discussed in Thread: ADS8698

Hello,

I have issues to communicate with the ADS8698EVM-PDK with an Arduino Uno over SPI.

The connections on the digital interdace I made are the following:

- DAISY, grounded trough J2;

- REFSEL, grounded trough J4;

- RST/PD, i didn' t "get" this signal from anywhere;

- AVDD, i provide 5V trough pin 2 of j32;

- DVDD, I provide 5V trough pin 2 of j33;

- A0+, I connected it to a 3.3V signal.

The voltages on AVDD, DVDD and REFIO are correct. The code I use is the following:

#include "SPI.h"
//ADS8698 pins
const int cs = 10;
//mosi = 11 (SDI)
//miso = 12 (SDO)
//sck = 13 (SCLK)
const int _RST = 9;

#include "SPI.h"
SPISettings ADS8698(8000000, MSBFIRST, SPI_MODE1);

void setup() {
pinMode (cs, OUTPUT);
pinMode (_RST, OUTPUT);
digitalWrite(_RST, HIGH);

delay(10);
Serial.begin(9600);
Serial.println("Test");
delay(1000);


//SPI.beginTransaction(ADS8698);
SPI.begin();
//ADS8698 starts with all channels enabled.
//ADS8698 starts with PGA's set to +/- 2.5*Vref. (LSB = 78,125 uV)
digitalWrite(cs, HIGH);
digitalWrite(cs, HIGH);
digitalWrite(cs, LOW);
SPI.transfer16(0x8500); // reset
digitalWrite(cs, HIGH);
digitalWrite(cs, HIGH);
digitalWrite(cs, LOW);
SPI.transfer16(0xA000); //auto mode
digitalWrite(cs, HIGH);    

}

void loop() {

for (byte i = 0; i < 4; ++i){
 
delay(10);
digitalWrite(cs, LOW);
SPI.transfer(0x00);
SPI.transfer(0x00);

byte MSB = SPI.transfer(0x00);
byte midSB = SPI.transfer(0x00);
byte LSB = SPI.transfer(0x00);
 
uint32_t result = (MSB << 16) | (midSB << 8) |LSB;
result = result >> 6;
         
digitalWrite(cs, HIGH);             
Serial.print("CH");
Serial.print(i);
Serial.print(": ");
//Serial.println(result);
Serial.print(MSB, HEX);
Serial.print(",");
Serial.print(midSB, HEX);
Serial.print(",");
Serial.print(LSB, HEX);
Serial.print(": ");
Serial.println(result);

delay(5000);
  }
}

  • Hello Tim,

    This is the third post you have written about this issue. It is easier to help you if you remain on only one post. This was we can follow what actions you have already tried and continue to move forward.

    As stated in your previous post A scope shot on your digital communications would be the best way to debug, if you would provide one we can take a look at your digital signals.

    RST/PD is active Low, make sure this pin is pulled high in normal operation.

    Regards

    Cynthia