This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP92066EVM: USB2ANY

Part Number: LMP92066EVM
Other Parts Discussed in Thread: USB2ANY, LMP92066

I have two set of LMP92066EVM with USB2ANY board.  One of them is have some problem. 

When I tried to use one USB2ANY as a standalone device, the software, USB2ANY Explorer-2.8.2.0 ,  displayed error message and asked me to upgrade its firmware. After I upgraded its firmware, the USB2ANY module can be detected and all functions, DAC, SPI and I2C  are working now.

But, this USB2ANY cannot work with my LMP92066 device anymore.  When I connect it back to LMP92066 amd run LMP92066 GUI software, it always shows that I2C devices not found, and the green LED on USB2ANY module is off.

I have verified that my LMP92066EVM is good if I use a new USB2ANY module removed from another working LMP92066EVM.

Can you tell me how I can load the original firmware back to my USB2ANY?  Do you have any firmware can support both LMP92066EVM and standalone SPI, I2C, DAC and ADC device?

Thank you

Xing