Part Number: LDCCOILEVM
Other Parts Discussed in Thread: LDC1614
Tool/software: WEBENCH® Design Tools
Hello,
I used the Webench Coil Designer to recreate coil Q from the LDC reference coils set, since I'm trying to implement it in a design in Eagle 9.0.1.
When exporting the file, I didn't get a schematic (although the readme.txt referred to using it) and tried to use the .brd and .scr to put the coil in my designs, but it didn't work.
I followed the steps in a different thread with the LDC1000.zip, but that only gives me 9 consistency errors with "schematic and board are not consistent".
I also tried using Eagle 7.1.0, but without success, it gave the same errors.
Also, when I downloaded the LDCCOILEVM Design file to get the schematic of coil Q into Eagle through the gerber files, it seems I am missing something to get it to work?
What do I need to do to resolve this issue?
Kind regards,
Ricardo A. Rodrigues