A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1251 Other Parts Discussed in Thread: ADS1254
Hello! ADS1251 was used for data collection Now the MCU power supply USES 3.3v. In order to avoid the problem of level matching, I want to use 3.3v power supply for ADS1251. Is that ok? thank you!
The ADS1251 only operates off of a single 5V supply and the digital interface is also 5V logic. You'd need to use a level-shifter to interface with a 3.3V MCU.
You might consider the ADS1254 instead... It allows for a second digital supply source and can interface with 3.3V logic. It also has a built-in multiplexer and allows for four differential inputs.