This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLABS-SAR-EVM-PDK: ??

Part Number: PLABS-SAR-EVM-PDK

Is there a way for the user to define and apply a window shaping pattern to the collected data? Using either "None" or "7 Term B-Harris" is rather limiting.

  • In older ADC Evaluation Module software interfaces we listed a wide range of windows (e.g. Hann, Hamming). We have found for ADC characterization with a single sinusoidal input frequency that the 8 term Blackman Harris is the most effective at reducing the spectral leakage.  For this reason, we limited the choices to Blackman Harris and no window.  No window was kept in place in cases where coherent sampling is used.

    Art

  • In the case of coherent sampling, is it possible for me to clock the ADC with an external clock to do the coherent sampling or can the PSI module be configured to coherently sample the 2 kHz test signal? Where can I find this information?

  • The PHI (digital controller) has an SMA connector that is intended for a clock input. In the future, we plan on developing firmware to allow for this functionality but presently the firmware / software doesn’t work for this.  The PSI (signal generator) also has the same plan for future development of external clock input for coherent sampling.  Long story short, we don’t have this capability now but plan for it in the future.

    Sorry that I can’t provide this functionality now. One key point: using the 8 term Blackman Harris we are able to achieve very good performance characterization on 18 and 20 bit converters.