Part Number: DAC8760
Dear Specialists,
My customer is encountering the same problem.

Could you please see attached file below.
In his case, output current is 19.8mA when DAC8760 is set to 20mA.
According to the shread, the error comes from gain error, 0.21% x 0.016 =0.0336mA, it's far from 0.2mA
The reverse current of Schottky diode and TVS diode is 0.01 uA.This is not still sufficient to 0.2mA.
What else can be considered as a factor of the error?
I appreciate your great help in advance.
Best regards,
Shinichi