Part Number: AFE4300
hello,
I am using the afe4300 with stm32 . I was reading the datasheet regarding spi and it says there are 24 bits to be sent, in which starting from MSB 21st bit is read or write bit and five bits after that 20:16 are for address. But for standard SPI there must be six bits for address. Also the bit 22 and 23 have not been mentioned. So they should be made 0?