This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5282: ADS5282 along with FMC-ADC adapter in spartan 6 device

Part Number: ADS5282


I am working on a project that involves SP605 xilinx eval board and an ADS54RF63EVM ADC eval module (along with the ADC to FMC passive adapter board).  I'd like to capture ADC output and send it out of the gigabit ethernet interface on the sp605.  Would the code you are providing here help with that?  Could you please send it to me so I can evaluate it?  Thank You all in advance