Part Number: ADS4242
Other Parts Discussed in Thread: TMS320C6748
Hi,
We are testing the high-speed signal processing application as ADS4242 + TMS320C6748(upp port).
But there is the phase difference between 1ch and 2ch of ADS4242 at 4.096MHz sampling rate, 5kHz input frequency.
The phase difference is from 0.48-degree to 0.9-degree, it's like delaying or omitting the output clock(1-clock to 2-clock),
and all data(1ch/2ch), sampling frequency are no problem.
What's a root cause of this problem?
Is the sampling of 1ch and 2ch implemented at the same time, simultaneously?
If yes, share me with the detailed document.
Please refer to the bellow schematics.
Regards,
Jeffrey