Other Parts Discussed in Thread: ADS7828
Hello,
I plan to use the ADS7828-Q1 ADC in my design. However, I am a bit confused about the input ranges in differential / single-ended modes and about the typical application "8.2.1 ADS7828-Q1 With Current Shunt Monitor" which is detailed in in the datasheet.
1/ From the datasheet page 4 (6.3 Recommended Operation Conditions) and the video "SAR ADC Input types" from TI (https://training.ti.com/ti-precision-labs-adcs-sar-adc-input-types, I understand that the ADS7828-Q1 has pseudo-differential inputs : negative input (VIN-) must remain between -0.2V...0.2V. However :
- In Figure 25, VIN- is connected to a 3.3V reference voltage.
- In datasheet page 22, it is written "The fully differential voltage input of the ADS7828-Q1 device..."
Which kind of input has this ADC : pseudo-differential or fully-differential ? Can VIN- go a few volts above GND ?
2/ In Section "8.1.1.3 Single-Ended Inputs", it is explained that in single-ended mode, one bit of resolution is lost because only half of the input scale is covered. This would be true for a fully differential input ADC, not a pseudo-differential input. The datasheet of the ADS7828 (not ADS7828-Q1) doesn't mention this at all. On top of that, in Figure 24, we can read "Output Codes 0-32767" although this ADC has only 12 bits.. This makes me think that this whole section of the datasheet is wrong.
In single-ended mode, is one bit lost ?
3/ In this post https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/695297, Abhijeet wrote that "For single ended configuration (Input referred to COM pin), analog input range is up to VDD. ". This means that VREF isn't used in single-ended configuration ?
In summary, my questions are :
- In single-ended mode
- Is VREF or VDD used to define the LSB ?
- Is one bit lost ?
- In differential mode :
- Is the input pseudo-differential or fully differential ?
Thank you,
Thomas