Is there any setting available withing TVP5158 to reduce rise time of CLOKOUT Pin.
We are using two TVP5158 and cascading mode and using single crystal part# FH2700019Z (Pericom) to feed 1st TVP5158.
Taking CLKOUT from 1st TVP5158 and feeding to 2nd one as input source clock.
We are also taking two 8-bits parallel output from each TVP5158 which is running @ 108MHz.
During FCC testing, we have observed that it is radiating at 27MHz, 108MHz, 379.9MHz,
Is there any setting posibsle withing TVP5158 to control its rise time of output PCLK and CLKOUT signals to reduce its rise time?
-Kartik