This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A04: ADS131A04 F_FRAME fault

Part Number: ADS131A04

Hi,

I am using ADS131 in my data acquisition device. ADC works fine, I am pretty happy with it. After initial debugging I have noticed that in the status word after transmission bit 6 is high. According to the datasheet it means that there is an SPI related problem. After investigation of the STAT_S (0x05) register content I saw that only bit 0 is set. It corresponds to message: Not enough SCLKs are sent per frame.

Some details about my implementation: no hamming code, 24 bit word, asynchronous slave mode. Fixed word size is disabled, no CRC (checked in the 0x0C register). I use MCU with SPI to read the measurements. ADS131 provides me with 4 24 bit measurements and 24 bit status word (padded with zeros). I use 8 word long FIFO on MCU side, with FIFO word is 2 bytes long. This means that after DRDY provides ready signal MCU inserts enable, CLK signals for 128 (8*16) clock cycles (I write zeros to MOSI in order to keep SPI active). ADC needs 5*24=120 clock cycles to send all bytes. If I didn't miss anything it should be enough to read all data.

As I have mentioned measurements look good I have no problem. I am just wondering why ADS131 sets this alert. I attach below scope screenshot, it can be seen that truly enable signal (dark blue) and clock (light blue) are active longer than ADC is sending data (MISO is violet). Sampling frequency is 20.830kHz.

BTW, ADS131 doesn't have programmable offset calibration, yes?

Thanks in advance.