Other Parts Discussed in Thread: TMS320F28377D
Hi TI experts,
We are interested to use ADS8588H as an external ADC to be interfaced with delfino MCU (P/N : TMS320F28377D).
Please share application notes for interfacing ADS8588H with any Delfino MCUs,if available.
Also,pls let me know which pin can be treated as WRITE BAR pin in the below diagram.
Also,i need to have Pin to Pin matching solution using ADS8588H with the existing ADC(MAX1312). Pls refer the below schematic & suggest the hardware connections.
regards,
Ramesh P