This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
ADS4122 data sheet (SBAS 520 C) page 13
Analog Power ADS4122, ADS4142 (125 MSPS): 112 mW
It is stipulated in.
The ADS4122 and ADS4142 are specified with 65MSPS. (page4 5.Device Family Comparison)
For this reason, I think that the devices written in the 112mW section are ADS4125 and ADS4145.
Is this a mistake?
※ Also Digital Power, LVDS Interface, low LVDS swing section,
Similarly Digital Power, CMOS interface, 8pF external load capacitance, fin = 2.5MHz
Also Standby.
It is also a mistake and I think that it is correctly ADS4125, ADS4145 (125MHz).
best regards
cafain
Cafain,
You are correct. This is a typo in the data sheet. This will be corrected in the next release of the data sheet.
Regards,
Jim