Part Number: DAC8551
Other Parts Discussed in Thread: DAC161S055, , DAC8811, DAC8811EVM, OPA277
Team,
We are trying to understand the device parameters that gives or influence the frequency of the output signal.
Goal is to find out what is the maximum frequency the a DAC could output.
Requirement is to be able to go up to 50kHz.
-Is the settling time the major parameter to look at?
Are there other parameters?
Can all three DACs (DAC8551, DAC8811, DAC161S055 : comparison of those DACS) enable to generate a clean 50 kHz signal?
-EVM: Which one of those DAC would enable an easy evaluation on a Win7/Win10 PC?
It seems that the dac811evm-pdk
Thanks in advance,
Anthony