Part Number: ADS8684
Hello,
I have a customer that has 2 questions about the ADS8684 device.
- On page 8 the "Offset error temperature drift" parameter. Is ppm/°C the same as µV/°C? So if you wanted to calculate the maximum offset error at a certain temperature would you multiple the offset error temperature drift by the number of degrees from 25°C you want. Take this and add and subtract it to the max offset error at 25°C (EO)? The customer wants to make sure that this is not with reference to AVDD, DVDD or the reference voltage.
- From the customer: What is the accuracy of the actual reference used by the adc? Not the level appearing on the REFIO pin. At the top of page 10 it just states Vref = 4.096 (internal) without any tolerance, which is incredible UNLESS the tolerance is perhaps already taken into account in the various offset and gain tolerances. In other words, perhaps we take “4.096” as a 0-tolerance number, knowing that whatever tolerance it actually has will be accounted for when we do our calculations of gain and offset.
Thanks you in advance!
John