This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5474EVM: Max no damage analog input power to ADS5474EVM J11

Part Number: ADS5474EVM

What is the maximum no damage analog input power in dBm (50 ohm source) into the ADS5474EVM for a 500 MHz 400 ns pulse?  I need to select a limiter to reduce a radar transmit pulse bleed through into the ADS5474EVM while still obtaining near full scale input power on low level radar reflected signals.