This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC900-Q1: Design a PCB with DAC900-Q1

Part Number: DAC900-Q1
Other Parts Discussed in Thread: DAC2900, DAC900, DAC900EVM, SN74LV245A

Hi TI expert,

I've designer a PCB with DAC2900, 125MHz clock, based on your EVM file's instructions. Now, I decide to turn to DAC900-Q1, 165MHz clock. 

My DAC2900 works well. Its clock is fed by FPGA's PLL and its 10 inputs are buffered by R-pack.

An EVM file is provides for DAC900 or DAC900-Q1.But, unfortunately,  this file hardly provides any detailed componnet usage or PCB's schemtic. 

I wonder if I apply my schematic designs of DAC2900 to DAC900, will this work? And is such R-pack very neccesary? Considering my application requeires high clock rate, but input data changes relatively slow, at a change rate of once per 100 nanoseconds.

Regards

Yatao