Part Number: ADS1232
Hi,
We are using ADS1232 for weighing scale application and is working fine. The issue is that the data count is not stable. When we power on the board we are reading the ADC count and displaying the weight and if we keep the board on for long run test the weight value slowly start decreasing. We have observed that when the room temperature increases the ADC count value decreases and when the room temperature decreases the ADC count value increases.
I have attached schematics for ADC. In the actual board we assembled C321 and C322 doe additional filtering on input voltage. The gain is set to 128 from controller. On power up we are calibrating the ADC by providing the additional clock on SCLK.
C308 and C316 (C0603C104K4RACTU) are ceramic capacitor. The filtering feed through capacitors uses is NFM21PC105B1C3D from Murata. We have followed the schematics from ADS1232REF. On the PCB there are no tracks routed below the ADC and has a good ground pour around the ADC.
We are averaging 4 samples and taking 20 bits for removing the noise from the ADC count. Please do let me know if you need more info.
Thanks,
Sreekanth