Part Number: DAC161P997
Other Parts Discussed in Thread: DAC161S997
I have a converter which converts 24V(loop+) to 5v and a LDO which converts 5V to 3.3V. Something happens without a reason like letting output pin of DAC(loop-) float or connecting it to ground throug 100ohm or sometimes when i connect device to power source it starts drawing much more current then useal. but this is not for sure i did all of these things 100 times and nothing happened 99 times.anyway if everyhing stops working. when i check the voltage difference between loop- and those converter's outputs, i see a voltage around 20V.But it is more likely loop- is -20V(negative) And if i change DAC with new one everything is OK. and oddly nothing gets damage because of this.