Part Number: DAC5682Z
Other Parts Discussed in Thread: DAC5674
I am currently working on a University project, and would like to use the DAC5682Z.
I have read the datasheet and the user guide for the evaluation board, but there are Things i do not understand, which I was hoping you Guys could help explain.
I want to use the DAC in dual mode, and as I understand it the data input is a mixed I/Q signal. If I want the two DAC's to output different data with 160 MHz how should I setup the clock inputs? Do I need two clock inputs, one with a frequency of 160 MHz, and one with 320 MHz? Is it somehow connected to the internal interpolation and/or PLL option?
What if I want the option between 1 or 2 DAC's can I use the same clocks as mentioned before?
Michelle