Part Number: ADS7844
I'm attempting to use the 24 clock cycle model to communicate with the device (Figure 3 in user's manual) but I never seem to get any data back from the device during the 16 clock cycles "Conversion". I do however see data in DOUT while I'm sending my 8 bit command word. The screenshot below shows me requesting data for CH0, single ended.
Setup:
Vref=3.3V; Vcc=3.3V; SHDN/=3.3V; Clock Speed = 1 MHz