This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DAC3XJ8XEVM software Installation is fine.
But while opening application lot of LabVIEW front panel module missing error pops up.
USB connection failed.
Installed: DAC38J84 GUI Ver 2.1
Jagadeesh,
Yes there is a chance that the GUI is not supported on Windows 10, because the GUI uses LabVIEW 2010 Run-Time engine which is not compatible on Windows 10. (i.e., NI doesn’t guarantee the functionality of LabVIEW 2010 Runtime engine in a Windows 10 PC)
But when we tried to install the GUI in a Windows 10 PC, we were able to run the GUI without any issues. So it seems to be a PC specific issue. There is a possibility that the software is not installed properly.
Can you try the following:
1. Uninstall LabVIEW 2010 Run Time Engine and the DAC3XJ8XEVM GUI.
2. Install LabVIEW 2010 Run Time Engine from the following link: http://www.ni.com/download/labview-run-time-engine-2010-sp1/2292/en/
3. Install and run the DAC3XJ8XEVM GUI.
Regards,
Jim