Part Number: ADS8588H
Other Parts Discussed in Thread: OPA365, OPA836, ADS8528, ADS8568, ADS8568EVM-PDK
Hi TI experts,
I am looking for a suitable OPAMP buffer for ADS8588H with input voltage range +/- 10V.
For other details & requirements about ADS8588H,pls refer the following thread which i already posted.
I understand from the following link for selection guidelines of OPAMP buffer for ADC.
https://www.changpuak.ch/electronics/Choosing_OPAMP_to_drive_ADC.php
Pls suggest a suitable OPAMP buffer with higher CMRR,higher bandwidth & +/-10V operating range.
I have located some options like OPA365,OPA836,TLO84 etc.
But none of above are satisfying my requirements to meet +/-10 V input range.
Kindly held me to locate right OPAMP BUFFER for the selected ADC - ADS8588H.
regards,
Ramesh P