Part Number: TLV5614
Hello team,
TLV5614 is used on a mass production project. About 1% of TLV5614 will have a problem that before MCU configure TLV5614 via SPI bus, the analog output OUTA~OUTD of TLV5614 will output 5V voltage (analog power supply of chip is 5V), which leads to abnormal operation of the machine.
The TLV5614 of the normal working machine analog output OUTA~OUTD output is 0V voltage before configuration. Replacing faulty chips to good machines can cause the same problem.
Further research found that the chip's AVDD power is power on 4 ms earlier than the DVDD, and the failure disappeared when the power on sequence was modified to DVDD first.Referring to the specifications of TLV5614, no description of the timing of power-up was found.
Does TLV5614 have clear requirements for power-on timing? Is the TLV5614 chip that output abnormal damaged?
Thanks